Other Parts Discussed in Thread: UCC28C56EVM-066
Tool/software:
Hello,
what is the exact purpose of R8 and D10 in UCC28C56EVM-066?
I know that D10 is there for overvoltage protection. If Vout is above 18V it will be conducting, limiting the output voltage. However theres no resistor limiting the current, so I guess D10 will be destroyed in an overvoltage event?
Also, the datasheet specifies the maximum output voltage as 19.3V at no load, isnt D10 always conducting when theres no load at the output then?
Regarding R8, maybe its purpose is to discharge the capacitors?
See attached image.