Tool/software:
Dears,
My customer use BQ24610 for 6S Li battery, input power want to use 28V adaptor.But the output voltage accuracy of the 28V adapter is 2%, which means the ripple voltage will reach 28.5V, which exceeds the maximum Vin range of BQ24610(28V).If a 27V adapter is used, this specification is not a standard voltage and requires customization, which will be much more expensive. The customer still hopes to use a standard voltage adapter of 28V. May I ask if a 2% accuracy 28V adapter can be used for the voltage input of BQ24610? Thanks