Tool/software:
Hi,
I am designing isolated DC to DC converter for EV 2w/3w automotive application with following specification.
Electrical: DC-DC Converter (72V to 12V)
Input Voltage: 72V (45 to 90V)
Output Voltage: 12V ± 0.1
Output Current: 20A
Output power = 300W continuous
I am at the beginning stage of design, I will be interested to know the suggested parts from TI power portfolio with reference design.
I have selected UCC28781-Q1 which has a ref design for 600W however input voltage is 370 V to 410-V DC.
Thank you