This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100EVM-795: Accuracy of bq35100 voltage reading?

Part Number: BQ35100EVM-795
Other Parts Discussed in Thread: BQ35100

Tool/software:

Hello I've calibrated the voltage for my bq35100 device wit open circuit load. It's within 10mV in the open circuit condition...but it's around 150mV when a load is used (aroud 250mA of current flowing)...Is this to be expected? 

What is the expected accuracy?


As a side question. Our current board does not have the ability to drop the load current to zero for voltage calibration. Any issues with incrementing/decrementing the offset with current flowing to obtain the calibration..?

This would be accurate in the flow conditions but possibly off in the no-flow condition...thoughts?