Part Number: BQ25620
Other Parts Discussed in Thread: TPS61032, TPS610333
Tool/software:
Hi there,
Currently, I'm designing a power circuit for my portable device. I'm exploring if BQ25620 could be used in my use case. I see that the IC has a OTG boost converter, which outputs 5V, and this is exactly what I need, but I'm not sure if the OTG is designed to use this way? I can use output from SYS, but I'd need to boost it externally, so I'd like to avoid it.
If it's not possible, can you suggest a similar IC that has a proper boost converter that I can feed into my system?
Some details and requirements about my project:
- USB-C powered (no PD), with up to 500-1000 mA current need for the system
- Li-ion/li-po battery, ~1000mAh
- MCU's Vin is rated 5-17V
Thanks!