This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2553: schematic review

Part Number: TPS2553

Tool/software:

Hi team,

My customer uses TPS2553 as a simple power protection device.

Could you help check the schematic below?

Another question is, can Fault signal control EN shutdown IC when OC occurs? Thanks 

  • Hi Jimmy,

    1.  If connected as shown, the switch will only provide 75mA of typical current before going into current limit.

    2.  C62 is not functionally necessary and should be removed.

    3.  a 0.1uF capacitor should be added to the IN pin (1)

    4.  It is not necessary to connect the EN pin (3) to /FAULT.  The switch will turn off in fault conditions.  I suggest directly connecting it to the IN pin (1) instead

    Regards,

    Chuck

  • Hi team,

    1.  If connected as shown, the switch will only provide 75mA of typical current before going into current limit. 

    A: Yes. Customer just use the device to protect their system. 

    2.  C62 is not functionally necessary and should be removed.

    A==> Got it.

    3.  a 0.1uF capacitor should be added to the IN pin (1)

    A==>Got it.

    4.  It is not necessary to connect the EN pin (3) to /FAULT.  The switch will turn off in fault conditions.  I suggest directly connecting it to the IN pin (1) instead


    A==> But I saw datasheet shown enter current limit during output short.until thermal shutdown then tune off the FET. instead of turning off FET directly when output is short. right?

  • Hi team,

    Any update?