This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62843: TPS62843

Part Number: TPS62843


Tool/software:

When input voltage drops to the same level as output voltage, the duty cycle is 100% and output = input. My question is, what if the input drops a little lower (say by 100mV) - does output follow the input, or buck convertor stops functioning ( which means I will need to switch to buck-boost).

Thank you.