Tool/software:
I have an isolated power supply design based off the 23755 reference design. The POE power is working correctly. I see it drop to the lower voltage when the secondary power supply is connected. But when I remove the secondary supply, the switching stops and the chip gets hot and never works again.
What could be causing the failure? I have adjusted the setpoint resistors to give a 15V output instead of a 12V output. Otherwise the circuit is the same as the reference design.