Other Parts Discussed in Thread: TLV61220, TLV61070A
Tool/software:
hi Sir
I survey the LTC3400 to do the circuit, also see TI have a TLV61046a, does they P2P?
and, may i know how the efficiency of TLV61046A in Vin 1.8V; Vout =5V/250mA
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
TLV61046A is p2p with LTC3400. But the max Iout of TLV61046A is around 160mA when Vin = 1.8V and Vout = 5V.
TLV61070 can output 250mA when Vin = 1.8V and Vout = 5V with efficiency > 85%. It's not p2p with TLV61046A.
I'll further check whether there are better p2p choices.
Regards
Lei
Hi Alex,
The efficiency is around 70% for TLV61046A when Vin = 1.8V, Vout = 5V, Iout = 160mA.
Regards
Lei
Hi Alex,
ILTC3400 can't output 250mA when Vin = 1.8V, Vout = 5V. The max Iout is around 150mA.
There is no device that p2p with LTC3400 and better efficiency. TLV61070A and TLV61220 are the most close devices, although they are not p2p.
Regards
Lei