Part Number: UCC27624
Tool/software:
Hi team,
We are Using UCC27624 drive transformer, the ratio of the primary and secondary turns of the transformer is 1:2, and 0.1A electronic load is loaded on the secondary side, and the heating UCC27624 is serious and soon reaches more than 100 °C

White is the unloaded OUTA output waveform, and green is after 0.1A load
My questions :Is it normal to heat up after adding 0.1A load, the specification is the ability to ± 5A, and the second is how to keep the output voltage of OutA constant after loading?
Thankyou