Other Parts Discussed in Thread: TPS22908
Tool/software:
I am starting a project that requires a single "3.2V" (2V-3.65V) LiFePO4 18650 cell to be in a housing with exposed contacts, I will refer to this a the "battery pack", which is intended to be easy to swap in and out of the unpowered device. The device will only be battery-powered, the batteries will be charged by a dedicated charger outside the device, so this is not a "hot-swap" scenario. The plan is to use spring contacts to connect the battery to the device. The battery cell will be charged at 2.5A max and discharge with 1A max.
My concerns/thoughts I'm hoping for clarification/feedback on are...
- On PCB of the device, to protect from reverse-polarity during battery insertion, I am considering using TI LM66100. In the datasheet for the LM66100, 8.3.1 shows reverse polarity protection RPP. Also on that same page, 8.3.2 shows reverse current blocking RCB. Looking at both of these, I it seems the reverse current blocking approach shown in 8.3.2 will also provide reverse polarity protection, is this correct?
- On the PCB inside the "battery pack" am hoping to add short-circuit protection. It needs to allow for bi-directional current so I can charge the battery in the charger. Does TI offer an IC that can provide short-circuit protection in the battery pack? Perhaps an eFuse or similar?
- When connecting the battery pack to the device with spring contacts, I'd like to protect the device against voltage spikes or other power anomalies. Does TI offer an IC that is intended to protect an unpowered device during battery insertion? I am considering an inrush-current limiter of some kind. Many of TI's hot-swap controllers do not support the voltage range of LFP cells 2V-3.65V. A possible candidate that I've found is the TPS22908, but maybe there's a better option?