Other Parts Discussed in Thread: BQ76942, BQ25756
Tool/software:

Hi Team,
Attached is an image showing the block diagrams of two ICs used in our system. Our project is a power bank with a 240 Whr capacity, configured with a 5S4P cell arrangement. Each cell has a capacity of 3350 mAh.
I am trying to charge the system with a 100W input, as depicted in the image.
The ICs we are using are:
- BQ25750 - Charger IC
- BQ76942 - AFE IC
I have a few queries:
- The BQ76942 recommends using multiple MOSFETs in the power path, specifically in a parallel configuration for both CHG and DSG FETs. However, this configuration is not applied in the BQ25750 IC, where only a single MOSFET is used. Why is there a difference in the MOSFET configuration between the AFE IC and the Charger IC while they are using similar kind of power paths?
- What are the calculations or considerations behind choosing these MOSFETs?
- Are the multiple MOSFETs used for reducing power dissipation/Losses?
- What is the specific purpose of using multiple MOSFETs in the AFE IC?
Thank you,
Apurva
Senior Embedded Hardware Engineer