The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5163: Load step down overshoot for LM5163

Part Number: LM5163

Tool/software:

During load transient of 400mA to 0mA I have observed voltage overshoot approx. 5.5V (0.5V additional for approx 50ms) at output of diode.

My configuration of buck converter is shown in below snap : 

The purpose of diode is to protect output from external voltage and aditional zener and diode at feedback will protect FB pin in case of overvoltage. to avoid diode loss feedback is taken after diode.

Specifications and desined parametersare :

Vin 12V Typ

Vout 5V

Iout max 400mA

L selected 100uH

Cout 40uF

Cin 20uF

RA 25K

CA 24nF

Cb 2nF

RF1 20k

RF2 6.34k

Circuit works as expected only during load step down voltage after diode has overshoot of 5.5V for approx 50ms ? Is there any way to reduce this overshoot ? does it mean controller not acting fast enough to bring down output voltage low by driving low side switch ? Is there any relation of this with ripple network ?

Thank you.