Part Number: TPS25830-Q1
Tool/software:
Hi team,
Could you teach me how to calculate eq(7) about R_ILIMIT.
Are these three parameter (R_SET, R_SNS, I_LIMIT) should use typical value?

Regards,
Youhei MIYAOKA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25830-Q1
Tool/software:
Hi team,
Could you teach me how to calculate eq(7) about R_ILIMIT.
Are these three parameter (R_SET, R_SNS, I_LIMIT) should use typical value?

Regards,
Youhei MIYAOKA
Hello Youhei,
Yes, 15mΩ for R_sns and 300Ω for R_set are the recommended values to be used for the TPS25830-Q1. Therefore, these values should also be used for Equation 7.
If the desired current limit is 3.3A, for example, Equation 7 yields 11.9kΩ.
Hope this helps,
Seong
Hello,
Yes, the accuracy of the current sense is dependent on the R_ilimit, R_set, and R_sns resistor parameters such as tolerance, temperature coefficient, resistor composition, and operating temperature. The goal is to minimize the variance of the resistance, especially at high ambient operating temperatures.
Also, short parallel traces from the CSP and CSN traces to the shunt resistor will yield the best performance. A small filter capacitor in parallel with R_sns and a small filter capacitor from CSN/OUT to AGND can also help decouple noise.
Hope this helps,
Seong