Other Parts Discussed in Thread: CSD18542KTT
Tool/software:
Hello Ti Team,
I have build the prototype board based on BQ7791514PWR.
My battery nominal voltage 12.8V, 6Ah, 4 cell in series, Below is the schematics.
The Problem is:
1. I have added 10K POT resistor to simulate the NTC temperature. I am getting total series cell voltage 13.01V on the Battery pack terminals, (BAT+ and BAT-)
But when i create a fault by varying the Pot resistor, It is showing ~10V, not going to 0V.
I have below power MOSFET for charge and discharge control. Can you please check where it went wrong.
Which resistor value i need to change get to 0V, when fault created.
| Q5, Q6 | Texas Instruments | CSD18542KTT | MOSFET N-CH 60V 200A DDPAK |
Your quick response is highly appreciated.
Regards,
-Ravi.
Regards,
-Ravi.