This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56628: VREG5 voltage is high

Part Number: TPS56628

Tool/software:

Hi team,

I had built a circuit with 12V input and 5V output, but when I put in an input voltage of 10V or more, the voltage dropped by about 2.5V and it stopped working properly.
After investigating various failure points, we confirmed that the voltage at VREG5 was high (about 8V).
We believe that this phenomenon is caused by the destruction of the built-in LDO.
Are there any possible causes for the breakdown?

Sincerely,
Ryu