This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8262EVM: How to decrease the temperature rise of the chip when driving TEC

Part Number: DRV8262EVM
Other Parts Discussed in Thread: DRV8262

Tool/software:

Hi- team,

My customer use DRV8262  to drive the TEC 12V@4A, they test it with our EVM. When drive 2 * TEC with 1 DRV8262 for about 30 mins(Line3 &4 in the table), the final temperature is about 55℃ under ambient temperature.

Consider the actual condition, the ambient temperature maybe 40-50℃, which means our device goes to 70℃. 

1. Customer wants to make the temperature <60℃ without heatsink. Do you have any suggestion to solve it?

2. I find there are some vias under the chip in the EVM. Do we Resin Plug Hole or fill the hole with copper?

3. for the dead time of DRV8262, is it constant to be 300ns? Is there a way to adjust the dead time?

4 Do we have any TEC testing report using DRV8262 that can share with customer?

5 How to select the value of the capacitor on VM? Is there a formula that can refer to? 

Thanks a lot

Matthew