Part Number: TPS22919
Other Parts Discussed in Thread: TPS22950
Tool/software:
Hi,
Would like to check if there is a load switch with short circuit current limit lower than 900mA (preferably <600mA), and able to do lower sequencing (OQC and EN pin).
Currently we are evaluating the TPS22919 and if possible we would like the short circuit current limit to be lower than that if possible.
1A, or even lower, max continuous current is sufficient for our application.
Seek your advice.
Thank you.
Regards.