Part Number: CSD18511KCS
Other Parts Discussed in Thread: CSD17573Q5B, CSD17570Q5B, CSD18531Q5A, CSD18533Q5A, CSD18543Q3A, CSD88537ND, CSD18535KTT, CSD18540Q5B, CSD18536KCS, CSD18536KTT
Tool/software:
Hello Team,
We are looking for some high current MOSFET for one of our products.
Hope your team can help us on this.
The MOSFET driver we are using will be TPSI3050 in the following configuration.

1). The high current can be bidirectional so we are using back to back MOSFETs.
2). The VGS voltage will be 10V.
3). Low RDSon is needed.
4). Low ON capacitance between the D-S pins.
5). The continuous current will be just above 40A and will be 100% time ON.
6). We cannot parallel multiple MOSFETs because of the space constraints in the PCB
7). Most MOSFET datasheet/vendor sites says their MOSFET is able to carry hundreds of amperes. But when we dig deep into the datasheet, we can see some conditions like package limited, or silicon limited or not meeting the SOA.
8). Can anyone suggest a MOSFET for our application?.
9). Is there any method to measure the RDSon of the MOSFET. In the datasheet of some MOSFETs (CSD18511KCS) the RDSon will be marked as 2.6mOhms.
Is there any method to measure the RDSon using multi meter.
When we measure the resistance across the drain and the source we get the resistance as 300mOhms.
But when we measure the voltage drop across the VDS and when I divided it with ID, i got the RDS as 200mOhms.
We have another application in the same board with continuous current of 15A.
Can you suggest another MOSFET for this application.
Looking for your reply.