Tool/software:
Please share the PSRR graphs for Buck 1, 2 and 3. Also share the value of maximum allowed ripple at the input of all the bucks and LDO (PVIN_B1, PVIN_B2, PVIN_B3 and PVINLDO).
Kindly share the PDN for reference.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Please share the PSRR graphs for Buck 1, 2 and 3. Also share the value of maximum allowed ripple at the input of all the bucks and LDO (PVIN_B1, PVIN_B2, PVIN_B3 and PVINLDO).
Kindly share the PDN for reference.
Hi Muthugomathi,
PSRR usually apply to LDO only not to any BUCKs.
The value of maximum allowed ripple at the input of all the bucks is to make sure the input is in this range: VINmin>UVLO_fall (set by NVM) for BUCK1 and 2.5V for Bcuk2 and3; and VINmax<18.3V for BUCK1 and 5.5V for Bcuk2 and3.
Thanks!
Phil
Thanks for your response.
Actually we are using the buck output for analog power supplies. That is why we need the ripple rejection ability of the bucks.