Other Parts Discussed in Thread: LP8758
Tool/software:
Hello expert,
Could you provide the replacement for A4001 from Aerosemi? I checked the spec from customer side and A4001 is 4-ch 4Apeak/ch PMIC. And the Vin is 2.7V to 5.5V. Customer's requirement is shown below.
CH1 : 0.9V / CH2 : 1.2V / CH3 : 1.8V / CH4 : 3.3V. I'm asking for current but it should be lower than 2A per channel. Is LP87564-Q1 suitable for customer? If no, please kindly help to share your comment to us. Thanks a lot!
Best regards,
Ann Lien