Part Number: TPS61099
Other Parts Discussed in Thread: TPS61299, , TPS610985, TPS61299A
Tool/software:
Hi TI team,
We are designing an application with the following design configuration.

Basically, the design includes 2x batteries Li/SOCl2 using an ORing configuration, a MCU and a radio and a Sensor IC that requires a minimum voltage of 3V and a maximum operation current of 2mA.
In this case we think that a boost converter configuration would fit our design best.
Maybe we could get your help to find something that suits us.
Maybe the TPS61099 or the TPS610993 Vout = 3V, for better efficiency. The TPS61299 seems to be recent/improved but we are not sure about the efficiency for the same voltage configuration because only the Vout=5V is described in the datasheet.
The TPS610985 also seems very interesting in terms of efficiency.
Also some other device could be recommended.
However, it would be important to consider the following points:
- When the Vin > Vout, Vout should follow Vin and show a low quiescent current.
- It starts operating with seamless transition when the input voltage decreases approaching the configured 3V output.
- High efficiency current under a light load considering that the current of the sensor IC in idle mode is ~5.25uA. So, something in this range is expected.
- High efficiency when operating assuming that the sensor IC has a maximum current of 5mA.
Please let me know if some additional clarification is required.
Thank you for your support