This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS631010: Differences from TPS631000

Part Number: TPS631010
Other Parts Discussed in Thread: TPS631000

Tool/software:

Hi support team,

When comparing the datasheets for TPS631000 and TPS631010, I found the following differences.

Device: TPS631000, TPS631010
Package: SOT-583, WCSP
Abs(Min) of Input voltage for less than 10 ns (LX1, LX2): -0.3V, -2.0V
Output voltage (Max): 5.3V, 5.5V
Thermal Information

Are there any other differences?

Why is the IReverse specification not listed for TPS631010?

The biggest difference is the package, so should I use them depending on my package preference?

Regards,
Dice-K