Tool/software:
Hello. - Hello.
I am evaluating BQ51050B with bq51050BEVM-764.
I have gradually increased the temperature from 10°C to 20°C, and the bq51050BEVM-764 does not start charging.
When the charger is turned OFF and then ON, the bq51050BEVM-764 starts charging.
Similarly, the temperature is gradually lowered from 70°C to 20°C, and the bq51050BEVM-764 does not start charging.
When the charger is turned OFF and then ON, the bq51050BEVM-764 starts charging.
I control the temperature by adjusting the R3 of the bq51050BEVM-764.
Is this bq51050B behavior in accordance with the specifications?
I expect the charger starts charging, when the temperature goes above 0°C.
I also expect it to resume charging, when the temperature drops below 60°C.