This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: BQ28Z610-R1, low temperature operation inquiry

Part Number: BQ28Z610-R1

Tool/software:

We sloved 'SOC jump down issue at -20°C' by changing register.

Previously we proceeded getting chemistry ID, Cycle learning, Resistance Temperature Compensation Optimizer in order.

But SOC jump down issue was not solved. So we applied hysterisis method by changing register like below

<Register Action>

Action No.

Address

NAME

Below -5°C

0°C or more

1

0x45BE

Term Voltage

3400mV -> 2800mV

2800mV -> 3400mV

2

0x45C3

Term Min Cell V

3000mV -> 3100mV

3100mV -> 3000mV

3

0x464D

IT Gauging Configuration

16ce

14ce

Our system cut-off voltage is 3400mV but our cell is dropped to 3300mV when loading 700mA at -20°C. So SOC was dropped to 0% and powered off as soon as loading current in 1minute.

But when I set Term Voltage enabled, set this to 2800mV, SOC dropped issue was disappeard and possible to load 700mA continuously about 3 hours.

However I wonder whether it is the right workaround that I applied

If you need logs or settings, ask me anything

Thanks