This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25018: Current limited buck project progress

Part Number: LM25018


Tool/software:

Hi everyone.
I'm revisiting the link as it's been a while. I tested the LM25018 because I needed a buck that would convert the Vin (20-28V, nominal 24V) into 16.8V very stable and with a limited current.
My request was to have very minimal current and voltage fluctuation and this chip was recommended to me. I tested it and however I encountered a problem: the current limit beyond which I didn't want the load to go was 350mA but this chip has a much higher current limitation from the datasheet which can even reach 750mA which is more than double the desired .
1) Is there a way to limit the current?

2) Otherwise, is there another buck (with all integrated MOSFETs), perhaps with the same package and similar layout, that can satisfy my request for current limitation on the output to a maximum of 350mA? What can you advise me?
Thank you