Part Number: TPS61165
Tool/software:
Hello !
I got couple of LED drivers, driven from 4V Li battery. Most of them work well (output current 60mA is correct, wave is rectangular) but one has very erratic waveform with overshoots and output current does not go over 17mA)
Even the changing of IC and inductor and output diode does not change anything. Inductor goes very hot, normally its only slightly warm.
I have checked the PCB million times. Could there be some inherent design instability ? I have tested other supplies with input voltage 3.3-4.2 and different loads (22 to 30V LED strings)
It must be something obvious. Looks like the IC output does not turn on correctly ?
Please help :)