This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317: LM317

Part Number: LM317

Tool/software:

Need to have a reference circuit for using LM317 as constant current of 1mA.

application - will be use to sense temperature from PT100 sensor. (3 wire)

Voltage used is AA battery - 3V.

  • Please follow the applications circuit in fig 18 of the datasheet and use a 1250Ω resistor at the output instead of 24Ω. This sets the output current to the desired 1mA. Connect the RTD to where the battery is connected in this schematic. Input and Output capacitors are not required. Please note that the minimum recommended output current for this device is 10 mA and you shall be operating below this limit.