This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92638-Q1: Turn indicator is off when the input volage is at 16V to PCBA

Part Number: TPS92638-Q1

Tool/software:

Dear Sir,

We are using the TPS92638QPWPRQ1 IC in two of the locations (U1 & U2)  of our LED PCBA .There are two test points connected with pin 8 (fault pin) of this IC.There are two test point connected with Pin 8 of U1 7 U2,Whenever we touch this TP15 or TP25,the turn indicator is not glowing and when we restart the power supply the turn indicator is working fine.There is one capacitor location in LAM PCBA (c26) when we short this capacitor c26,all the turn indicator function at 13.5V or 16V is working fine.I can share the schematic for both LAM and LDM PCBA .Please check the schematic and please let us know design flop if any,