This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH-CIRCUIT-DESIGNER: LM51561H-Q1PWP

Part Number: WEBENCH-CIRCUIT-DESIGNER

Tool/software:

i am planing to designing  two dc-dc  converters using Webbench power designer tool 1) non isolated DC-DC converter specifications is input voltage iminimum 3.3V and maximum 5V, output is 15V and 15A current max

2) Isolated DC-DC converter input voltage 15V and output is 3.6V and  out put current is 20A,

for above designs I  used  these IC''s 1)LM51561H-Q1PWP IC used for isolated power supply

2)LM34936RHF IC used for non isolated power supply.

3)my orginal design specification is input 3.3  to 5V and output is 3.6V and current 75W  but i did n't get any isolated design, so for that reason I will planing to integrate the two above designs one is  non isolated+ isolated.

is it correct approach to design, please let me know  and below i have attached these two schematics urls.1) file:///C:/Users/Admin/Desktop/VSSC/Isolated%20Schematic.svg.

2) file:///C:/Users/Admin/Desktop/VSSC/Non%20isolated%20Schematic.svg.