Part Number: TPS65094
Tool/software:
Hello:
I used your TPS650940A0RSK for Intel Apollo Lake design. We produced 10 boards, and one of the boards had a power failure in the system. It appears to be a power drop on the 1.8V output (BUCK4) causing the PMIC to have no output.
Problems with the welding or the chip itself can be ruled out for now. Because it is good at the beginning, it can work normally, and this problem occurs after a period of aging. The maximum temperature of the IC was 45.1℃ at normal temperature 25℃ and 68.4℃ at 60℃. The chip has problems when used at room temperature, which should have nothing to do with temperature. I would like to analyze what causes it. Could you please give me some ideas on how to solve the problem?