Other Parts Discussed in Thread: LM5022, , UCC28065, UCC28070, LM5122
Tool/software:
What is the range of the input and output voltage?
input voltage: 20V ; output voltage: 50V ,operating in CCM mode could it be possible?
And do TI have the IC that is boost interleaving ? The function is like LM5022, but I need interleaving.
Thank you!
simplified diagram to design my project?