This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5155-Q1: Recommend boost controller(analog)

Part Number: LM5155-Q1
Other Parts Discussed in Thread: LM5155, UCC28180

Tool/software:

Dear Ti

I hope TI recommand Boost controller below conditions

type: no isolation type(or possible isolation type)

boost switching freq: lower freq 30kHz ~higher no limit

Vin(dc): 60Vdc min ~ 311Vdc max

Vout(dc): 500Vdc

boost duty: no limit(i hope below 95% or designed circuit below 95%)

Power device: no limit(Si SiC Gan FRD Anything)

Pout: 400Wmax(60Vdc/500Vdc) ~ 2600Wmax(311Vdc/500Vdc)

function1: boost en/dis(on/off) < i will control it with gpio of mcu(ex c2000)

function2: automotive

function3: use external isolation or high power gate driver + power device SiC(~1200V) or GaN(~650V)

Best reguards. Choi