This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSI2140-Q1: block diagram misunderstand in datasheet

Part Number: TPSI2140-Q1


Tool/software:

Hi team,

My customer  have some misunderstand about VM pin connection. look like VM is connect to center of two back to back MOS, so can it use as two channels switch? I mean VM pin use as another switch input like S1/S2.

Regards,

Amber

  • Hello Amber,

    Thanks for checking with our team. The SM pin cannot be used as a two channel switch. The purpose of this pin is to allow for thermal dissipation within the device.

    With this in mind, we currently offer the TPSI2072-Q1, which has two enable channels that each control a single back-to-back FET.

    If you have any more questions, please let us know. 

    Regards,

    Jose

  • Hi Jose,

    but I'd like to know why look like VM is connect to center of two back to back MOS?, it will misunderstand others from datasheet block diagram

    Thanks.

    Regards

    Amber

  • Hello Amber,


    For TPSI2140-Q1, the SM is electrically connected to the common-source of the center MOSFETs. However, the device does not have independent enable signals. The device is designed to turn on/off all MOSFETs from a single enable signal. This is the reason it cannot be used as a two-channel switch.

    Can you provide more context on the exact application from the customer, is this a concern? And why they would like to configure it as a two channel switch?

    As mentioned before, if they do require two independent paths, TPSI2072-Q1 will be a better fit. 

    Regards,

    Jose Rojo