This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090-Q1: I2C Address Response

Part Number: UCD9090-Q1

Tool/software:

Hi Team,

With 2x UCD9090-Q1 in the system, the PMBus_ADDRx resistors are as follows:

Device 0:

Expected Address: 0x34

PMBus_ADDR0: 31.6kOhm

PMBus_ADDR1: 31.6kOhm

Device 1:

Expected Address: 0x41

PMBus_ADDR0: 41.2kOhm

PMBus_ADDR1: 41.2kOhm

However, when they run an I2Cscan in Linux on this I2C bus, they only get responses from addresses 0x0C and 0x7F. Even with an 8bit vs 7bit adjustment that doesn't explain these two responses. Do we know if there is any reason the UCD9090-Q1 would respond to 0x0C or 0x7F?

Thanks,

Justin