This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM63615-Q1: +/-1.5% tolerance includes resistor tolenance

Part Number: LM63615-Q1
Other Parts Discussed in Thread: LMQ61460

Tool/software:

Hi team,

I am looking for a automotive battery input to 8.5V output with 1.5% output voltage tolerance for 400mA output. 

Most of the high accuracy DCDC converter achieve 1% reference, but it cannot meet total 1.5% tolerance even if I use 0.5% tolerance resistor divider. 

Could you please advise if there is +/-0.5% tolerance DCDC converter (Adjustable out) or +/-1.5% fixed 8.5V output converter? 

Or is there tracking WVIN DCDC converter? 

regards,