Part Number: TPS3435-Q1
Other Parts Discussed in Thread: TPS3430, TPS3435
Tool/software:
Hi TI,
I've been developing a system to be latched using an external open drain buffer based on the application note: snva837.
In this document, the implementation is based on the TPS3430, but my own judgement decided that the implementation of both the TPS3435-Q1 and TPS3430 are similar.
Im using the TPS3435AFACADDFRQ1
While testing I haven't found the latching functionality working at all.
I'm using the next values for my components:
- Crst = 2.2nF.
- Cwd = 10nF.
- 10k pull-up resistor after WDO*.
- SET0 = 0.
- VDD = 3V3.
When testing I find that the capacitor is just charged by the Crst pin, but in my understanding when asserted the open drain buffer SN74LVC1G07DBVR should keep Crst from being charged which latches the whole system.
Do you have any suggestions as to why this latching functionality isn't working?
Kind Regards,
Max