This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65220: PMIC Device failing to initiate power

Part Number: TPS65220

Tool/software:

Hi,

We are using the TPS6522053RHBR IC in our board with 3.3V input. 

We have referred to the AM64xx eval board for schematics.

But the PMIC is not powering up on our board. We have checked the status of the few control pins as are as below:

VDD1V8 - 1.8V

VSEL_SD/VSEL_DDR - 3.3V

MODE/RESET - 3.3V

MODE/STBY - 3.3V

nRSTOUT - 0V

nINT - 3.3V

But we are seeing none of the outputs are coming up. Please find the schematics page attached.

PMIC-Page.pdf

Please help us with the debug points if any.

Thanks & regards,

Nanjunda M