This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21040: Different charging current for different input voltages

Part Number: BQ21040


Tool/software:

Hello All,

We are using BQ21040 to charge LiPo battery with charging current of 150 mA from a  input supply of 5V. The resistor value of 3.6K was chosen for that.  Ts terminal was connected to 10K resistor as temperature sense functionality is not required.

When we give 5V to VIN pin, input current is around 122 mA (Believe this is same as charging current). When we reduce voltage slowly, input current is increasing and when the input voltage is around 4.6V input current reached to 150mA.

Initial battery voltage is 3.6V and as battery charges, if input voltage is kept at 5V, input current is 122 mA till battery voltage reaches to 4.2V and then entering to constant voltage mode. But current never goes to expected 150 mA.

Can anyone help me understand what could be happening?

Thanks

Ravi