This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Stefan,
1. OVP can also trigger if the voltage goes over 4.2V for over a second. You can try measure the voltage at the pins of the device over the period of time or watch it over an oscilloscope to ensure that’s not the case. Also, is the discharge FET also turned off? If so, that would imply OCC.
2. The body diode of the CHG FET allows current to still be pulled from the load even though the CHG FET is turned on.
Best Regards,
Alexis H.
Hello again!
1. The discharge FET is turned on. I've measured each cell and it triggers once a cell hits exactly 4.0V
2.So there is no issues with the OV test? it is supposed to act that way? I find it weird that during other fault detections, both current and voltage drops close to zero but not in this case.
Best,
Stefan
Hello Stefan,
Best Regards,
Alexis H.