Tool/software:
hi,
Question 1:The STAT pin of BQ24163 is connected to the LED light, and charging is input from USB. Whether the current is 1.5A or 100mA, after charging for a period of time, the LED light will turn off. In less than an hour, unplug the USB, plug it in and power it on again, and the LED will light up again; When the LED light is off, the STAT pin voltage is around 2.5V, while the battery voltage is only 3.5V. The customer uses a lithium battery with a full charge voltage of 4.2V. The schematic diagram is shown below. Please help analyze the reason;

Question 2:After the customer writes the chip address 6B through IIC, the chip responds and then reads the chip address 00 register. However, the chip does not respond, so the data cannot be read, the waveform is shown below, please help analyze the reason;

Thanks!