Part Number: UCD3138OL64EVM-031
Other Parts Discussed in Thread: UCD3138
Tool/software:
Development Board: UCD3138OL64EVM-031
CCS Version: V12.7.1.00001
Compiler Version: v5.2.9
JTag: XDS110V2
I am using the new development board, UCD3138OL64EVM-031, and I have already enabled the JTAG functionality using PMBus.
I followed the video "Using JTAG with the UCD3138: Overview of programming options" from the link below to set up the UCD3138 target configuration:
www.ti.com/.../introduction-to-digital-power-controllers.html
However, when erasing the flash, it seems that the erase data flash is missing, leading to an error message during the subsequent blank check. This prevents normal execution of the following debug process.
Is there any way to solve this issue? Or is there any JTAG-related documentation you can share?
erase flash and blank check:

try to load program: