Part Number: LM137QML-SP
Tool/software:
Hello,
The datasheet 6.1 states as follows.
PDmax = (TJmax - TA)/RθJA, and TJmax = 150oC.
PDmax at TA=25oC for T0-39 = 2.5W.
Here, RθJA is calculated as follows.
RθJA = (TJmax - TA)/PDmax = (150 – 25)/2.5 = 50 (oC/W)
However, the datasheet 6.4 states RθJA is 174(oC/W) (still air @0.5W), and 64 (oC/W) (500 LFM @0.5W), so both are different from 50(oC/W) calculated above.
How the PDmax @25oC is calculated as 2.5W?
Best regards,
K.Hirano