Tool/software:
Hi there!! As I have no previous experience with switching voltage converter ICs, I'd like to ask if there are any special precautions to be taken in order to power hifi audio equipment.
I plan to use a 10uF/10v MLCC ceramic (0805) cap (for C1) and to further minimise the power supply footprint
a few 47u/10V 0805 MLCCs. Also a 680uH choke from the output of the chip to the rest of the circuit. Are there any inrush current issues?
Any precautions during startup or power off?
Do I need to put any flyback diode in parallel with the choke? Are there any voltage spikes regarding the IC operation?
I have attached a quick schematic of what I plan to do. Let me know if there are any issues that I have to be aware of.