Tool/software:
Hello Team,
I am working on UCC14341-Q1 IC. I want to understand more detail on UVLO. At same conditions, IC is going to auto recovery and sometimes to latch-off mode.
. Protection mode, auto-recovery. In this mode, the module is off, due to the input UVLO or OVLO protection. After the input voltage fault is cleared, depending on the ENA pin voltage condition, it either becomes disabled mode if the ENA pin voltage is low, or it goes through soft-start mode to the normal operation mode.
5. Protection mode, latched-off. In this mode, the module is off, due to other protections. The module remains off even the fault causing the protection is cleared. Recycling VVIN operation must ensure the input voltage goes below the analog UVLO falling threshold (VVIN_ ANALOG_UVLOP_FALLING ) first to reset the latch-off state, or the ENA pin is toggled Low (OFF) then High (ON).
Could you explain in detail on this.
Thank you,
Tejasri.