Part Number: TPSM843B22E
Other Parts Discussed in Thread: TPS543B22
Tool/software:
Hello:
The datasheet does not really explain the GOSNS pin, which apparently stands for "ground sense return." The example on page 1 indicates GOSNS should just be grounded. The example on page 21 shows it apparently grounded through a jumper or optional jumper that is referred to as a "Net Tie" (name not explained). Figure 7-5 on page 15 indicates GOSNS drives the plus input of an amplifier named "RSA", while the FB drives the negative input. It is unclear if RSA is:
1. An op amp with unshown programming resistors to turn it into either an inverting amp or a differential amp that can be used differentially, or by setting GOSNS to ground convert that differential amp into an inverting amp.
2. Some other kind of amplifier.
My question whether some additional explanation can be provided that explains:
1. Was the grounding of GOSNS intended to be the main or only usage of the pin?
2. Is the jumper from GOSNS to ground intended to preserve some other use for GOSNS? If no other use is needed, should GOSNS just be grounded without bothering with the jumper?
3. Is RSA an op amp or some other kind of amp?
Thanks,
Farron