Tool/software:
Hi,
I've built a LED Driver Circuit using the LM3410 in the 1,6mhz version.
I'm driving 4 Leds with 2,8vf at 350ma.
My schematic is based on the Example 8.2.5 in the Datasheet.
I'm using a 16khz PWM Signal, but the LEDS start to light up with a duty cycle greater than 30 percent.
Reducing PWM Frequency helps a bit, but even at very low frequencies it doesnt seem to work properly.
At 1khz the leds turn on at 5% duty cycle.
Is this normal behaviour and related to the 20millisecond startup time?
Am i right, that the LM3410 regulates the output current instead of keeping it constant and applying the pwm signal to shut the led's on and off?
I need a high PWM Frequency, since the product is intended for film set lighting.
If there is a better option that takes Li-ion input voltage and works for 3 to 4 pieces of 1watt LED's, I'd also be interested to hear about that.
Thanks,
Markus Harthum