Tool/software:
Hi and thank you for your time reading this.
I am utilizing aforementioned TPS563200 in a ~12V input application targeting ~4.2V output.
I have followed guidelines presented in Datasheet version "SLVSCB0E – JANUARY 2014 – REVISED MAY 2023" sections 8.2.1 and 8.4.2. The results are close but not quite what I was hoping for. In particular, observed is a significant voltage drop as amperage increases, for example 1A draw brings it down to 3.34V.
Also observed is a minor squealing sound at low current draw, though I read this is to be expected
Please find attached Kicad schematics + layout (please ignore Q1 area as it is under revision)ENGH-36-v1.0.zip


No load
200mA load
400mA load