This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: Lead acid battery charger

Part Number: BQ25730

Tool/software:

Hello, Can I use the BQ25730 IC to charge a 12V lead acid battery and supply the system with PowerPath feature?

  • Hi, Pablo,

    Yes, BQ25730 is a multi-chemistry battery charger. You can simply set max charge voltage and charge current, then enable charging. It will charge the lead acid battery to the max charge voltage, and automatically transitions to the constant voltage charging. 

    You might need to terminate the charging operation when your target voltage is reached, by sending a command from a host or a MCU. 

    BQ25730 is a digital part, which relies on the host for communication. 

    I hope this helps. 

    Regards,

    Tiger