Other Parts Discussed in Thread: TPS63061
Tool/software:
Kindly review the schematic of Single cell Battery charger. You can ignore IP5306 circuit as it is not included in design. Basically We want to charge battery from USB-C and by using power path management of BQ24075 we will supply output to TPS63061. Which will regulate the output so that we will get fix 5V on output of TPS63061. And this 5V will be given to another USB-C for external power.
In previous design we directly used IP5306 and whenever we remove USB and system load shifts on battery, Power was getting disconnected for few seconds and our PCB was keep on resetting whenever USB and battery were switched. So that's why we removed IP5306 and added BQ24075 and TPS63061 combination.
You can also give recommendation of input and output USB-C connections. Thanks2112.Schematic1.pdf